You stop Enterprise Central to configure the port settings or to repair, upgrade, or reinstall Enterprise Central.
The Software Administrator installs with the Enterprise Server and Enterprise Central installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server and Enterprise Central.
Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation.
The Enterprise Server and Enterprise Central run in the background as Windows services. You start and stop the server services through the Software Administrator or Windows Service. Before shutting down a server, make sure the stop does not negatively affect your site.
The Enterprise Server and Enterprise Central use HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the server listens to when communicating through a specific protocol.
To configure a protocol port number, you first have to stop the running Enterprise Server or Enterprise Central service.
Port changes you have made using Software Administrator are not automatically updated in the Communication view for EcoStruxure BMS servers.
In Software Administrator , in the Enterprise Central view, click Stop Service .