Use the Enterprise Central view to start and stop the Enterprise Central service and configure the ports of Enterprise Central.
Enterprise Central view
Component |
Description |
Status |
Displays the current status of the Enterprise Central Windows service. |
Start Service |
Click to start Enterprise Central. |
Stop Service |
Click to stop Enterprise Central. |
HTTP Port |
Type the port number that Enterprise Central listens to when communicating through the Hypertext Transfer Protocol. |
HTTPS Port |
Type the port number that Enterprise Central listens to when communicating through the Hypertext Transfer Protocol Secure. |
TCP Port |
Type the port number that Enterprise Central listens to when communicating through the Transmitting Control Protocol. |
System |
Displays the system log. |
Path |
Displays the path to the folder where the Enterprise Central database and other objects created by Enterprise Central or users are stored. |
![]() |
A warning indicates that you entered a conflicting port number or that the service is stopping. |