earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
5/18/2018

Adding an Action Note to an Alarm in WebStation

You add an action note to an alarm to let others know what you have done to correct the problem that caused the alarm.

Show More
action_close

An action note is a predefined note that contains information on what you have done to solve the problem that triggered the alarm.

You can add an action note to an alarm. In some cases, adding an action note to an alarm is optional. In other cases, you are required to enter an action note when you acknowledge the alarm.

You add an action note using WorkStation or WebStation. You can view an action note added to an alarm in WorkStation or WebStation.

To add an action note to an alarm in WebStation
  1. In the Alarms pane, click the alarm.

  2. In the Alarm Details dialog box, click Notes .

  3. In the Notes dialog box, click Action notes .

  4. Click Add .

  5. Select the action note.

  6. Click OK .

  7. Click Close .

The action note is added to the alarm.

  • Action Notes
  • Alarm Details Dialog Box
  • Notes Dialog Box – Action Notes Tab