earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
5/18/2018

Adding a Check Mark to a Checklist in WebStation

You add a check mark to a checklist to show which steps you have completed to solve the cause of the alarm.

Show More
action_close

Checklists are predefined lists with steps you take to correct the cause of the alarm.

In some cases, adding a check mark to a checklist in an alarm is optional. In other cases, you are forced to add a check mark when you acknowledge the alarm.

You add a check mark to a checklist using WorkStation or WebStation. You can view the check marks added to a checklist in WorkStation and WebStation.

To add a check mark to a checklist in WebStation
  1. In the Alarms pane, click the alarm.

  2. In the Alarm Details dialog box, click Show checklist .

  3. Select the steps you have completed.

  4. Click OK .

The steps in the checklist are added to the alarm.

  • Checklists
  • Alarm Details Dialog Box