Functionalities: User Management
Product version: 3.2, 3.3, 2022
10/15/2020

Path Permissions Rules

A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Path permissions configured on lower levels of the path overrule permissions configured on higher levels.

Table: Software Permissions Rules

Property

Description

Read

Permits viewing and listing path content

Write

Permits an administrator to change configurations except for bindings, programs, and graphics

Create

Permits creating new objects on the path

Delete

Permits deleting objects under the path. Delete permissions are required on a folder to delete its contents

Edit

Permits editing objects on the path

Force

Permits forcing values on the path

Command

Permits the execution of commands on the path. Command permissions can override this permission for specific commands

Inherited

Indicates that the permissions are inherited from the parent folder

Note:

You need delete permissions to rename, paste and duplicate folders and objects in EcoStruxure Building Operation software.

Note:

You can always edit graphic and program objects in the relevant editor, however in order to save it on your server you need "Edit" permissions. You can save your edits on your hard drive or export to a location of your choice even if you don’t have “Edit” permissions.

Example

A user account group Janitors owns the permission Read to the /Trend_Logs path and the permissions Read and Write to its sub-path /Trend_Logs/Trend_Charts. Paul and Susan belonging to Janitors have a permission to modify configurations of objects in /Trend_Log/Trend_Charts sub-path, but can only view all the remining objects in /Trend_Logs path.

  • User Account Management Overview
  • Software Permissions
  • Path Permissions
  • Software Permissions Rules Management
  • Assigning Path Permissions to User Accounts or User Account Groups
  • Editing Path Permissions of User Accounts or User Account Groups
  • Removing Path Permissions from User Accounts or User Account Groups
  • User Account – Software Permissions Tab
  • User Account Group – Software Permissions Tab