The RP-C has fixed screw terminals for the power input, SSR outputs, relay outputs, high power relay outputs, and universal inputs/outputs.
The wiring recommendations are provided separately. For more information, see Wiring .
The RP-C-12A-F-24V model has 12 I/O points and the controller is equipped with 23 fixed screw terminals.
For more information, see RP-C-12A-F-24V Screw Terminals .
The RP-C-12B-F-24V model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
For more information, see RP-C-12B-F-24V Screw Terminals .
The RP-C-12C-F-24V model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
For more information, see RP-C-12C-F-24V Screw Terminals .
The RP-C-16B-F-24V model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
For more information, see RP-C-16B-F-24V Screw Terminals .
The RP-C-16A-F-230V model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
For more information, see RP-C-16A-F-230V Screw Terminals .
The RP-C-16B-F-230V model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
For more information, see RP-C-16B-F-230V Screw Terminals .