There is one LED on the front panel of the RP-C.
RP-C LEDs
Function |
Color |
Status |
Red, Green, Blue (and combinations) |
The RP controller Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK RP controller firmware application running No Bluetooth activity |
Blue, constant |
Normal operation, status OK RP controller firmware application running Bluetooth connection is active |
Green 3 seconds, blue 1 second |
Normal operation, status OK RP controller firmware application running Bluetooth advertising is active |
Green, flashing (~1 Hz) |
Device restarting, wait RP controller firmware application running |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
RP I/O board receiving software upgrade, wait Do not interrupt power to the controller. For more information, see the following Important note. |
Amber, constant |
RP controller firmware boot applet running |
Amber, flash |
Device restarting, wait RP controller firmware boot applet started |
White, transient |
Device starting, wait |
White, constant |
RP controller firmware not running, attention required (contact product support) |
Avoid interrupting power to the controller during the short period of time when the Status LED is flashing red and green. An interruption causes problems with the I/O processor upgrade, which can lead to corrupt firmware. The symptom of a corrupt I/O processor is often seen as the controller reporting itself as a “MP-C-15A”. A corrupt I/O processor can lead to loss of reset button functionality, loss of all I/O functionality, inability to upgrade the I/O processor, and/or inability to upgrade the controller.