earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebStation
Functionalities: Basic Functionality
Product version: 3.0, 3.1, 3.2, 3.3, 2022
7/18/2019

Log Pie

A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.

The Log pie can contain one or many logs. The colors and calculation method of every log can be changed.

Pie Center

The pie center can be used to display the following values:

  • None: Does not display any pie chart center.

  • Average: Displays the average value for all logs added to the pie chart.

  • Total: Displays the sum of all logs added to the pie chart.

  • Min: Displays the value of the log with the lowest value.

  • Max: Displays the value of the log with the highest value.

Numerical values

You can get a numerical display of all values in the log pie using the Display Values feature.

  • How Dashboards Work
  • Dashboard Widgets
  • Configuring a Log Pie