Product version: 3.0, 3.1, 3.2, 3.3, 2022
2/10/2021

Point Value Properties Dialog Box

Use the Point Value Properties dialog box configure and edit a point value.

 
action_zoom_plus_stroke Point value properties dialog box
Figure: Point value properties dialog box

Table: Point Value Properties Dialog Box

Component

Description

Add

Click to add a point.

Display variable

Enter the variable you want to display.

Icon

Select an icon to be displayed in front of the value.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

  • Dashboard Widgets
  • Point Value
  • Widget Dialog Box – Layout Tab