Product version: 3.0, 3.1, 3.2, 3.3, 2022
5/13/2019

Configuring a Point Pie

You configure a point pie to get a graphical presentation of the values in points in a pie chart.

Show More
action_close

A point pie chart is a circular graphic divided into slices to illustrate proportion of values.

The point pie can contain one or many variables. The colors and calculation method of every variable can be changed.

Pie center

The pie center can be configured as follows:

  • None: Does not display any pie center.

  • Average: Displays the average value for all variables in the pie.

  • Total: Displays the sum of all variables in the pie.

  • Min: Displays the value of the variable with the lowest value in the pie chart center.

  • Max: Displays the value of the variable with the highest value in the pie chart center.

Numerical values

You can get a numerical display of all values in the log pie using the Display Values feature.

To configure a point pie
  1. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  2. Click Add to add a variable.

  3. In the Display variable box, enter the variable you want to display in the point pie.

  4. In the Color box, enter a color for the variable.

  5. In the Caption box, type a caption.

  6. In the Caption Link box, enter a link to an object that is relevant for the point pie.

  7. In the Pie Center , select a pie center.

  8. In the Show Legend box, select True to display the name and color of the value in the point pie.

  9. In the Show Percentage box, select True to display the values in percentage.

  10. In the Display Values box, select True to display the numerical values of the variables in the point pie.

  11. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Point Pie
  • Point Pie Properties Dialog Box
  • Adding a Widget to a Dashboard