Show Abbreviated References

References in the List view are abbreviated to save space. An abbreviated reference might only display the first part of the reference but sometimes the last part is the most important one. You can have the system only show the last part of the reference in the list.

For example, if the full reference is ../../IO Resources/Onboard IO/DO 01 and you select to show abbreviated references, the list shows DO 01.

  • List View Toolbar
  • Basic Functions
  • Showing Abbreviated References