The IP-IO module comes in three models with different I/O point count and different I/O point types.
Model |
I/O Points |
Model |
I/O Points |
IP-IO-DI10 a |
10 |
IP-IO-UIO10 a |
10 |
IP-IO-UIO5DOFA4 a |
9 |
All IP-IO module models have the same small footprint.
The versatile mix of I/O point types match a wide variety of applications. The universal inputs/outputs are highly flexible and can be configured as either inputs or outputs.
Table: I/O Point Types by IP-IO Models
I/O Point Types |
IP-IO-DI10 |
IP-IO-UIO10 |
IP-IO-UIO5DOFA4 |
I/O Point Types |
IP-IO-DI10 |
IP-IO-UIO10 |
IP-IO-UIO5DOFA4 |
Digital inputs |
10 |
- |
- |
Universal I/O Type Ub |
- |
10 |
5 |
Relay outputs Form A |
- |
- |
3 |
High power relay outputs Form A |
- |
- |
1 |
The digital inputs can be used for sensing of multiple dry contact digital inputs in applications, such as equipment status monitoring or alarm point monitoring.
For more information, see Digital Inputs .
The universal inputs/outputs are ideal for any mix of temperature, pressure, flow, status points, and similar point types in a building control system.
For more information, see Universal Inputs/Outputs .
The relay outputs support digital Form A point types. The Form A relays are designed for direct load applications.
For more information, see Relay Outputs .
The main application of the high power relay output is to power an electrical heating element directly.
For more information, see High Power Relay Outputs .