earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: IP-IO
Functionalities: Hardware
Product version: 2022
12/17/2021

IP-IO Module Communication Ports

The IP-IO module contains a combination of Ethernet and USB communication ports.

This combination includes the following ports:

  • Two 10/100 Ethernet ports

  • One USB host port

  • One USB device port

When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. For more information, see Advantages to Using External Bindings . The second port also provides a connection point for a laptop running the Commission mobile application.

The two USB ports are reserved for future use.

  • Hardware Overview
  • IP-IO Modules
  • Advantages to Using External Bindings