earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Alarms
Product version: 3.1, 3.2, 3.3, 2022
12/19/2019

Alarm Toolbar

Use the Alarm toolbar to handle alarms in WebStation.

Table: Alarm Toolbar

Button

Description

 
action_zoom_plus_stroke

View settings

Select an alarm filter in the list. For more information, see Favorites .

 
action_zoom_plus_stroke

Show hidden alarms

Click to show hidden alarms. For more information, see Hide and Disable .

A yellow circle displays the number of hidden alarms in the alarm list.

 
action_zoom_plus_stroke

Show disable alarms

Click to show disable alarms. For more information, see Hide and Disable .

A yellow circle displays the number of disabled alarms in the alarm list.

 
action_zoom_plus_stroke

Filter

Click to filter alarms. For more information, see Temporary User Filters .

 
action_zoom_plus_stroke

Acknowledge

Click to acknowledge an alarm. When Acknowledge is active you can also mass acknowledge a number of alarms at the same time. For more information, see Mass Acknowledging Alarms in WebStation .

 
action_zoom_plus_stroke

Select all

Click to select all alarms in the alarm list. For more information, see Mass Acknowledging Alarms in WebStation .

 
action_zoom_plus_stroke

Deselect all

Click to deselect all alarms in the alarm list. For more information, see Mass Acknowledging Alarms in WebStation .

  • How Alarms Work
  • Hide and Disable
  • Temporary User Filters
  • Favorites
  • Alarms Pane and Alarm View