You connect to a device to begin all commissioning tasks.
In the Connection page, select WiFi .
In the Wi-Fi page, in the Adapter dropdown, select the IP address for your wireless adapter.
Configure the following optional features:
UDP/IP Port. The default port number is 47808. For more information, see IP Acquisition and Connectivity .
BBMD address. Enter the IP address here if you are connecting to a remote site. For more information, see IP Acquisition and Connectivity .
Select Connect .
In the Select BACnet Network page, the Commission mobile application automatically selects the local network. If you are connecting to a remote site, select the checkbox next to the appropriate network. Select Discover Devices .
In the Device List page, select the check box next to the device or devices you want to connect to. To select all devices listed, select Select All .
To filter the device list, select the Filter icon, and apply a filter. For more information, see Filtering the Device List .
Select Next .
Depending on whether you chose chose one or multiple devices in step 6, you will reach the following pages:
When you reach the Device Settings page, you have successfully connected to a single device.
When you reach the Download Firmware page, you have successfully connected to multiple devices.