earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Device Administrator, ​License Administrator, AS-P
Functionalities: Hardware, SmartDrivers
Product version: 3.0
5/13/2019

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

The Entitlements are added to the Device Administrator. After the Entitlements are added to the Device Administrator, you can view the products and then assign the licenses to the connected SmartX servers.

You can add one or many Entitlements to the Device Administrator.

After the purchase, the Entitlements are delivered in an e-mail.

Example

You have a site with five SmartX servers. You assume that the maximum number of WebStation clients simultaneously connected to each SmartX server at the same time are 10. Therefore, you need 50 client licenses. You want all SmartX servers to use SNMP notification and allow the users to create personal dashboards. Only two SmartX servers need SmartDrivers.

 
action_zoom_plus_stroke An example of an Entitlement.
Figure: An example of an Entitlement.

You can of course, at any time, buy a new Entitlement with new products that you add to your site.

  • Device Administrator Licenses