Use the Entitlements Product Licenses View to view automation server licenses.
Component |
Description |
Add entitlement |
Click to add an Entitlement. For more information, see Automation Server Licensing Overview . |
Add demo license |
Click to add a demo license. For more information, see Automation Server Licensing Overview . |
Refresh all |
Click to refresh the list. |
Product name |
Displays the product name of the product that contains the licenses in the row for the product. |
Activation ID |
Displays the activation ID. The activation ID is unique for the product and cannot be changed. |
[ License column] |
Displays the features that need licenses. For more information, see Software and Features that Require Licenses . |
Total |
Displays the product's total number of licenses. |
Available |
Displays the product's available number of licenses for the product that are not activated. |