There is one LED on the RP controller expansion sensor modules. The LED is integrated with the Set button.
Function |
Color |
Status |
Red, Green |
The sensor module Status LED can be configured in the following modes:
Show status mode
Off mode
You configure the Status LED mode in the EcoStruxure Building Operation software. For more information, see Configuring RP Controller Expansion Modules .
The sensor module Status LED indicates the condition of the device.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Normal operation, status OK. |
No action required. |
Green constant, with red flash (100 ms every 2 seconds) |
Normal operation, status OK. However, the sensor module has detected and logged an abnormal condition. When the RP-C has retrieved the diagnostics from the sensor module, the Status LED returns to constant green light. For more information, see RP Controller Expansion Module Diagnostics . |
No action required. |
Green, flashing (~1 Hz) |
Device is starting or restarting.
|
No action required. |
Green, flashing medium (~2 Hz) |
Device is in maintenance mode. For more information, see RP Controller Expansion Module Maintenance Modes . |
To exit the maintenance mode, configure a unique device address in the range supported by the RP-C controller model and then reset the device by disconnecting and reconnecting the device to the RP-C room bus. For more information, see Configuring the Room Bus Address for an RP Controller Expansion Sensor Module .For more information, see Connecting RP Controller Expansion Modules and Multi-sensors to RP-C . |
Green, flashing fast (~5 Hz) |
Device is initializing. |
No action required. |
Red, flashing (~1 Hz) |
Device is non-operational due to a detected error. Device is forced into maintenance mode. |
Contact Schneider Electric Product Support Services for assistance. |
Red, flashing fast (~5 Hz) |
Device is inoperable due to a detected, non-recoverable error. |
Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric. |
Red, constant |
Device is inoperable due to a detected, non-recoverable error. |
Return the device to Schneider Electric. |
The sensor module Status LED is disabled.