earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD
Functionalities: Hardware
Product version: 3.3, 2022
7/23/2021

Light Modules

arrow1_rotationRP-C-EXT-DALI-M-PD arrow1_rotationRP-C-EXT-DALI arrow1_rotationRP-C-EXT-0-10V-4-PD arrow1_rotationRP-C-EXT-0-10V-4

The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.

The light modules support different types of interfaces for lighting control. The light modules also come in different models with or without support for power distribution to the light control gear.

Module

Interface

Power Distribution

RP-C-EXT-DALI-M-PD

DALI

yes

RP-C-EXT-DALI

DALI

no

RP-C-EXT-0-10V-4-PD

0-10V

yes

RP-C-EXT-0-10V-4

0-10V

no

RP-C-EXT-DALI-M-PD

The RP-C-EXT-DALI-M-PD light module connects to the RP-C room controllers and provides I/O expansion for lighting control with DALI (Digital Addressable Lighting Interface).

For more information, see RP-C-EXT-DALI-M-PD .

RP-C-EXT-DALI

The RP-C-EXT-DALI light module connects to the RP-C room controllers and provides I/O expansion for lighting control with DALI (Digital Addressable Lighting Interface).

For more information, see RP-C-EXT-DALI .

RP-C-EXT-0-10V-4-PD

The RP-C-EXT-0-10V-4-PD light module connects to the RP-C room controllers and provides I/O expansion for 0-10V lighting control.

For more information, see RP-C-EXT-0-10V-4-PD .

RP-C-EXT-0-10V-4

The RP-C-EXT-0-10V-4 light module connects to the RP-C room controllers and provides I/O expansion for 0-10V lighting control.

For more information, see RP-C-EXT-0-10V-4 .

  • Hardware Overview
  • RP Controller Expansion Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-DALI
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-0-10V-4