Groups Substitution Codes

Groups substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the groups that are included in the notification report.

Table: Groups Substitution Codes for Notification Reports

Code

Description

@(ActiveScheduleValue)

Writes the value of the active schedule.

@(AutoLogOffInactivityTime)

Writes the time of the auto log off inactivity.

@(AutoLogOffToGuest)

Writes if auto log off will log on to Guest.

@(CommandPermissions)

Writes the command permissions of the group members.

@(Description)

Writes the description.

@(DomainName)

Writes the name of the domain the group belongs to.

@(GroupName)

Writes the name of the group.

@(IPAddressWhitelist)

Writes the whitelist of IP addresses.

@(MemberOf)

Writes which groups the group is a member of.

@(Members)

Writes the members.

@(Note1)

Writes a note for the event.

@(Note2)

Writes another note for the event.

@(PathPermissions)

Writes path permissions of the group.

@(Policies)

Writes policies of the group.

@(Schedule)

Writes the schedule.

@(ServerName)

Writes the server name.

@(TypePermissions)

Writes type permissions for the group.

@(WindowsGroupName)

Writes Windows Active Directory group name.

@(Workspaces)

Writes workspaces of the group.

  • Notification Reports
  • Alarms Substitution Codes
  • Events Substitution Codes
  • Multi Log List Substitution Codes
  • Properties and Watch View Properties Substitution Codes
  • Trend Log Records Substitution Codes
  • Users Substitution Codes