This section provides recommendations on wire sizes and lengths for the KNX Modbus gateway (RP-C-EXT-KNX).
The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
Terminals |
Minimum Cross-sectional Area |
Maximum Cross-sectional Area |
Maximum Cable Length |
Power input terminals a |
0.34 mm² (22 AWG) |
2.5 mm² (14 AWG) |
No limit |
Modbus terminals b |
0.34 mm² (22 AWG) |
2.5 mm² (14 AWG) |
No limit |
For more information, see KNX Modbus Gateway Screw Terminals and Connector .