Functionalities: User Management
Product version: 2022
12/17/2021

Property Permissions

Property permissions are used to give a user account group or a user account access to the properties of objects defined in the path. The permissions configured on the properties serve to refine permissions granted on the object level.

There are three levels of property permissions:

  • Inherit - Select to inherit permission to the property from the object.

  • Read-only - Select to give read-only access to the property.

  • Full control - Select to give full access to the property.

You to select the level of permission you want to assign to different properties. For more information, see Property Permissions Dialog Box .

  • Path Permissions
  • Software Permissions
  • Property Permissions Dialog Box
  • Assigning Path Permissions to User Accounts or User Account Groups
  • Editing Path Permissions of User Accounts or User Account Groups