Product version: 2022
12/17/2021

Alarm Sankey Chart Dialog Box

Use the Alarm Sankey Chart dialog box to configure and edit an alarm Sankey chart.

 
action_zoom_plus_stroke Alarm Sankey Chart dialog box
Figure: Alarm Sankey Chart dialog box

Table: Alarm Sankey Chart Dialog Box

Component

Description

Column

Select the column(s) you want to display in the widget.

Filter

Select the filter you want to apply.

Max number of nodes

Enter the number of bars you want to display in the chart.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Legend

Click True to display the name and color of the trend log in the widget.

Decimals

Select the number of decimals you want to display.

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab