earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Basic Functionality
Product version: 2022
12/17/2021

Configuring an Alarm Pie

You configure an alarm pie chart to get a circular graphic divided into slices to illustrate proportions of alarms.

Show More
action_close

An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.

Alarm pie displays all alarms in all states.

You can decide the alarms column you want to display. You can also apply a filter to select the alarms based on the alarm fields.

By clicking on a slice, you can view a list of alarms for that particular slice.

To configure an alarm pie
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Alarm pie properties dialog box, in the Column box, enter the alarm column you want to display.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the alarms.

  5. In the Max number of slices box, enter the maximum number of slices you want to display in the pie.

  6. In the Caption box, type a caption.

  7. In the Caption link box, enter a link to an object that is relevant alarm pie.

  8. In the Pie center select a pie center.

  9. In the Show Legend box, select True to display legends in the alarm pie.

  10. In the Show Percentage box, select True to display the values in percentage.

  11. In the Display Values box, select True to display the numerical values.

  12. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Alarm Pie
  • Alarm Pie Dialog Box
  • Adding a Widget to a Dashboard