earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2022
12/17/2021

Assigning a Value on Click

You assign a value on click so that you can give an event a value with one click in the Multi schedule viewer.

Show More
action_close

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

To assigning a value on click
  1. In WebStation, in the System Tree pane, click the Multi schedule viewer.

  2. In the Multi schedule viewer workspace, click the Settings button

     
    action_zoom_plus_stroke
    .

  3. Click Assign on click .

  4. In the Multi schedule value toolbar, enter the values you want to give the events.

  5. Click on the events that you want to give the values.

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace
  • Multi Schedule Viewer Toolbar
  • Creating a Multi Schedule Viewer
  • Adding a Schedule to a Multi Schedule Viewer
  • Removing a Schedule from a Multi Schedule Viewer
  • Adding the Same Event to Multiple Schedules
  • Opening a Schedule from a Multi Schedule Viewer