earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Basic Functionality
Product version: 3.3, 2022
7/22/2021

Outputs/Multi-State Detail Screen

Use the Outputs/Multi-State detail screen to display and edit the values available for the multi-state output.

Warning Warning

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Outputs/Multi-State detail screen

Outputs/Multi-State detail screen

Table: Outputs/Multi-State Detail Screen

Component

Description

Force

Tap Force to override the value received from the device. For more information, see Value Editing .

 
action_zoom_plus_stroke

Tap a value option. The value options differ depending on what the multi-state output is used for in the system.

  • Value Editing