Use the Edit exception event screen to add, edit or delete the time and value of an exception event.
Edit exception event screen
Component |
Description |
Value type |
Displays the schedule type the event is added to. For more information, see Schedule Types . |
Value |
Tap - or + to edit the schedule output value when this event is active. For more information, see Weekly Events . This field will be different if you have selected to edit a digital schedule event. |
All day |
Tap All day to make the event span 24 hours instead of selecting specific hours using From and To . |
From |
Tap - or + to edit the starting time of the event. |
To |
Tap - or + to edit the ending time of the event. |