Use the alarm detail screen to display the alarm details and to acknowledge the alarm.
Alarm detail screen
Component |
Description |
Device |
Displays the name of the device. |
Object name |
Displays the name of the input, output or value that activated the alarm. |
Object description |
Displays the description of the input, output or value that activated the alarm. |
Event state |
Displays the event state of the current alarm state. For more information, see Alarm Handling . |
Event state text |
Displays the event state text corresponding to the alarm state. For more information, see Alarm Handling . |
Transitions |
Displays a table that lists all the alarm state changes that has occurred. |
![]() |
Indicates an active alarm that is acknowledged. For more information, see Alarm Handling . |
![]() |
Indicates an active alarm in the state Fault that is not acknowledged. For more information, see Alarm Handling . |
![]() |
Indicates an active alarm in the state Alarm that is not acknowledged. For more information, see Alarm Handling . |
![]() |
Indicates a reset alarm that is not acknowledged. For more information, see Alarm Handling . |
Transition |
Displays the transition type. For more information, see Alarm Handling . |
Time |
Displays the date and time of the most recent alarm state change. |
Message |
Displays the alarm message corresponding to the alarm state. For more information, see Alarm Handling . |
Acknowledge |
Tap to acknowledge the alarm. For more information, see Alarm Handling . |