earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022
7/22/2021

Add Weekly Event Screen

Use the Add weekly event screen to create a new weekly event for a selected analog, digital, multi-state or enumerated schedule.

 
action_zoom_plus_stroke Add weekly event screen

Add weekly event screen

Table: Add Weekly Event Screen

Component

Description

Value type

Displays the schedule type the event is added to. For more information, see Schedule Types .

Value

Tap - or + to edit the schedule output value when this event is active. For more information, see Weekly Events .

Inactive/Active

Tap Inactive or Active (On or Off) to edit the schedule output value when this event is active. For more information, see Weekly Events .

All day

Tap All day to make the event span 24 hours instead of selecting specific hours using From and To .

From

Tap - or + to edit the starting time of the event.

To

Tap - or + to edit the ending time of the event.

Days of week

Tap to select the day(s) of the week this event is active.

  • Schedule Handling
  • Schedule Types
  • Weekly Events
  • Schedules Screen
  • Add Schedule Event Screen