earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2022, 2023, 2024
6/10/2022

RP Controller Expansion Zigbee Modules

arrow1_rotationRP-C-EXT-ZB-DALI arrow1_rotationRP-C-EXT-ZB-0-10V

The RP controller expansion Zigbee modules provide devices that can be used to form a connected room solution. The RP controller expansion Zigbee modules are connected to the RP-C room controllers through the Zigbee TM wireless protocol and provide the controllers with I/O expansion that enable lighting control.

 
action_zoom_plus_stroke RP controller expansion Zigbee module connected to an RP-C controller equipped with Wireless Adapter - Advanced
Figure: RP controller expansion Zigbee module connected to an RP-C controller equipped with Wireless Adapter - Advanced

RP-C-EXT-ZB-DALI

The RP-C-EXT-ZB-DALI Zigbee DALI module communicates with the RP-C room controller over the Zigbee TM wireless protocol and provides I/O expansion for lighting control with DALI (Digital Addressable Lighting Interface).

For more information, see RP-C-EXT-ZB-DALI .

RP-C-EXT-ZB-0-10V

The RP-C-EXT-ZB-0-10V Zigbee 0-10V module communicates with the RP-C room controller over the Zigbee TM wireless protocol and provides I/O expansion for 0-10V lighting control.

For more information, see RP-C-EXT-ZB-0-10V .

  • Hardware Overview
  • RP-C-EXT-ZB-DALI
  • RP-C-EXT-ZB-0-10V