This section provides information on regulatory compliance and approvals for the RS-485 Adapters.
The RS-485 Adapters include the following models:
Isolated RS-485 Adapter
Non-isolated RS-485 Adapter
The RS-485 Adapters bear the CE mark and complies with the following EU directives:
2014/30/EU Electromagnetic Compatibility Directive (EMCD)
2011/65/EU Restriction of Hazardous Substances (RoHS) Directive
2015/863/EU amending Annex II to Directive 2011/65/EU
The RS-485 Adapters and its packaging carry the waste of electrical and electronic equipment (WEEE) label, in compliance with EU directive 2012/19/EU, governing the disposal and recycling of electrical and electronic equipment in the European community.
The RS-485 Adapters bear the UKCA mark and complies with the following UK directives:
S.I. 2016/1091 - Electromagnetic Compatibility Regulations 2016
S.I. 2012/3032 - Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment Regulations 2012
The RS-485 Adapters are UL Listed Energy Management Equipment for the United States and Canada. UL file number: E526691.
The RS-485 Adapters comply with the following UL standards:
UL 916 - Standard for Energy Management Equipment
UL 2043 - Standard for Fire Test for Heat and Visible Smoke Release for Discrete Products and Their Accessories Installed in Air-Handling Spaces
Any changes or modifications to the products may invalidate the certificate.
The RS-485 Adapters bear the Regulatory Compliance Mark (RCM) and comply with the requirements of the relevant Australian Communications and Media Authority (ACMA) standards made under the Radiocommunications Act 1992 and the Telecommunications Act 1997. These standards are referenced in notices made under section 182 of the Radiocommunications Act and 407 of the Telecommunications Act.
The RS-485 Adapters bear the Environment Friendly Use Period (EFUP) marking of 20 years according to the Chinese RoHS as stipulated by the Chinese Ministry of Industry and Information Technology (MIIT).