You access License Server using the interface to configure the settings, for example, change the port number to the License Server.
On a computer that has access to the the same network as the License Server, to configure is located, open a web browser.
In the address field, type the License Server IP or network. End the address with a colon and then the port number.
License Server has the HTTP protocol through port 8888 set as the default. For example: http://162.192.10.1:8888
The default user name is: admin .
The default password is: admin .
For more information, click button Help button