Use the Modification submenu to manually add a trend log record or import trend log data from an .XML file to a trend log.
The trend log Actions menu, Modification submenu
Command |
Description |
Add log record |
Click to open the Add trend log record dialog box where you add values and comments to a manual trend log. For more information, see Manually Adding a Trend Log Record to a Trend Log .. |
Import log data |
Click to open an .XML file and import the log data to the selected trend log. For more information, see Importing Log Data to a Trend Log .. |