earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 1.0, 1.1, 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Activities Per User Report

The Activities Per User report provides information about some of the user activities for a particular user account. You can use the report to audit user activities such as creating and deleting objects, and completing successful logons.

The following table shows the input parameters for the report.

Table: Activities Per User Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the activity period.

End report date/time

Specifies the end date and time of the activity period.

Date range filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

User

Specifies the user account whose activities you want to audit.

Report view

Specifies the format, such as a table, for displaying the report.

Show top

Specifies a number used to filter the top most frequently occurring activities.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page