earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
12/14/2016

Adding a Checklist to an Alarm

You add a checklist to an alarm to troubleshoot the problem that triggered the alarm.

Show More
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

 
action_zoom_plus_stroke Checklist dialog box

Checklist dialog box

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To add a checklist to an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object to which you want to add a checklist.

  2. In the User Action view, in the Checklist box, enter the checklist you want to add to the alarm.

     
    action_zoom_plus_stroke
  3. Click the Save button

     
    action_zoom_plus_stroke
    .

To add a cause note to an alarm you must have created one in advance and defined its content.

  • Creating an Action Note
  • Create Alarm Wizard – User Action Page
  • Action Notes