earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
10/23/2018

Address Bar

Use the Address bar to browse the system. The Address bar is located at the top of the Workspace.

 
action_zoom_plus_stroke The Address bar

The Address bar

The Address bar is the equivalent of the Address bar in Windows and can be used for browsing the system and for copying addresses that you want to paste in other areas of the system, for example, in the Bindings View.

 
action_zoom_plus_stroke The Address bar

The Address bar

Table: The Adress bar filter

Button

Description

 
action_zoom_plus_stroke

Show/Hide non-presentation objects

Click to show non-presentation objects.

  • Showing Non-Presentation Objects in the System Tree Pane
  • Workspaces