Use the Address bar to browse the system. The Address bar is located at the top of the Workspace.
The Address bar is the equivalent of the Address bar in Windows and can be used for browsing the system and for copying addresses that you want to paste in other areas of the system, for example, in the Bindings View.
Button |
Description |
![]() |
Show/Hide non-presentation objects Click to show non-presentation objects. |