You can manage user accounts on a domain controller by logging on to the local domain of the EcoStruxure BMS server, using the local administrator and local reports administrator accounts.
Each EcoStruxure BMS server has a local administrator account, named admin. This account is preferably used to log on to the EcoStruxure BMS server the first time to create a new domain with an administration account. To manage and administrate the new domain, it is recommended that you log on to the domain with your domain administration account.
The local administrator account cannot be changed or deleted.
SystemReportsService is the user account for the Reporting Agent service. The account allows the Reporting Agent service to log on to the Enterprise Server. This user account is set up during the installation of the Enterprise Server and WorkStation and does not require any configuration.
The SystemReportsService is disabled in Enterprise Central and needs to be configured. The password also needs to be set before the Report Server is used with Enterprise Central.