earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 1.0, 1.1, 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Alarm Amount by Category Report

The Alarm Amount by Category report provides information about triggered alarms and organizes the information by alarm categories. Before you can generate report output for this report, you need to set up alarm categories in WorkStation and link alarms to the alarm categories. For example, you can set up door alarm categories or cooling alarm categories. You can then use the report to determine the problematic areas in your buildings such as the door alarms.

The following table shows the input parameters for the report.

Table: Alarm Amount by Category Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the triggered alarms.

End report date/time

Specifies the end date and time of the triggered alarms.

Date range filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Group interval

Specifies the time interval, such as daily, weekly, for organizing and displaying the number of alarms by category.

Target

Specifies a comparative value. When the report runs, the actual alarm counts by category are compared to the target value.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page