earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
5/19/2017

Alarm Objects in Multiple Servers

In a multi-server system, you create alarm objects on the Enterprise Server. These objects, such as checklists and action notes, are inherited by the SmartStruxure server devices that are connected to that Enterprise Server. The copies on the connected SmartStruxure server devices are read-only, so in order to edit them you must edit their source objects on the Enterprise Server. One advantage with this is that you can display the objects and their content on the SmartStruxure server devices even if the Enterprise Server goes offline.

Note:

When an Enterprise Server is connected to a SmartStruxure server device, all existing checklists, action notes, cause notes, and categories on SmartStruxure server device are removed and replaced with the objects from the Enterprise Server.

  • Alarms Overview
  • Multi-server System
  • Lead and Shadow Relationship