Use the Alarm Styles view to open the style properties of the different Alarm states.
Table: Alarm Styles View
Component |
Description |
Component |
Description |
Acknowledged Style |
Click to select the style object that configures the appearance of an acknowledged alarm in the Alarms pane and Alarm View. For more information, see Acknowledged Style Properties . |
Alarm Style |
Click to select the style object that configures the appearance of a triggered alarm in the Alarms pane and Alarm View. For more information, see Alarm Style Properties . |
Disabled Style |
Click to select the style object that configures the appearance of a disabled alarm in the Alarms pane and Alarm View. For more information, see Disabled Style Properties . |
Fault Style |
Click to select the style object that configures the appearance of an alarm with fault state in the Alarms pane and Alarm View. For more information, see Fault Style Properties . |
Reset Style |
Click to select the style object that configures the appearance of a reset alarm in the Alarms pane and Alarm View. For more information, see Reset Style Properties . |