earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool, WebStation
Functionalities: Alarms
Product version: 1.9
10/12/2017

Alarms Pane and Alarm View Icons

Use the alarm state icons in the Alarms pane and Alarm View to get information about the state of the alarms.

Table: Alarms Pane and Alarm View Icons

Icon

Description

 
action_zoom_plus_stroke

Normal

Indicates that the alarm is idle and the variable the alarm monitors does not satisfy the configured alarm criteria. For more information, see Alarm States .

 
action_zoom_plus_stroke

Alarm

Indicates that an alarm is triggered. For more information, see Alarm States .

 
action_zoom_plus_stroke

Acknowledged

Indicates that a user has acknowledged the alarm. The problem that caused the alarm has not been corrected. For more information, see Alarm States .

 
action_zoom_plus_stroke

Reset

Indicates that the problem that caused the alarm is corrected. A user needs to acknowledge the alarm to change the alarm state to normal. For more information, see Alarm States .

 
action_zoom_plus_stroke

Disabled

Indicates that the alarm is disabled by a user. Disabled alarms are by default hidden in the Alarms pane and Alarm View. For more information, see Alarm States .

 
action_zoom_plus_stroke

Fault

Indicates that the value reported from hardware, such as a BACnet device, is not trustworthy. For more information, see Alarm States .

 
action_zoom_plus_stroke

Attachment

Indicates that the alarm has an object attached. For more information, see Alarm Attachments .

  • Alarm States
  • Changing the Alarm State Sort Order
  • Alarm Attachments
  • Alarms Pane and Alarm View
  • The Alarm Is Disabled and Cannot Be Enabled