Use the alarm state icons in the Alarms pane and Alarm View to get information about the state of the alarms.
Icon |
Description |
![]() |
Normal Indicates that the alarm is idle and the variable the alarm monitors does not satisfy the configured alarm criteria. For more information, see Alarm States . |
![]() |
Alarm Indicates that an alarm is triggered. For more information, see Alarm States . |
![]() |
Acknowledged Indicates that a user has acknowledged the alarm. The problem that caused the alarm has not been corrected. For more information, see Alarm States . |
![]() |
Reset Indicates that the problem that caused the alarm is corrected. A user needs to acknowledge the alarm to change the alarm state to normal. For more information, see Alarm States . |
![]() |
Disabled Indicates that the alarm is disabled by a user. Disabled alarms are by default hidden in the Alarms pane and Alarm View. For more information, see Alarm States . |
![]() |
Fault Indicates that the value reported from hardware, such as a BACnet device, is not trustworthy. For more information, see Alarm States . |
![]() |
Attachment Indicates that the alarm has an object attached. For more information, see Alarm Attachments . |