Use the Assign Default Reports page to assign a template to a type of object. The template is then used when you generate a default report in WorkStation. For more information, see WebReports Main Page .
Assign Default Reports page
Component |
Description |
Type of Object |
Lists the type of objects associated with the templates. |
Default Report Templates |
Select to assign a template to a type of object. The template is used when you generate a default report. |