Use the Assignment properties to configure which user or user group receives the assignment request.
Assignment properties
Component |
Description |
Status |
Select Disabled to deactivate the assignment function. |
Schedule |
Enter the schedule or other multistate variable that contains the value that is to be used to activate the assignment. |
Active value |
Enter the value, generated by the connected schedule or other multistate variable, that is to activate this assignment object. |
Assigned to |
Click the browse button to open the Users and Groups dialog box where you select the EcoStruxure Building Operation user or user group to receive the assignment request. For more information, see Users and Groups Dialog Box . |