Use the Backup Options dialog box to select the EcoStruxure BMS server and the type of data that you want to back up. You can also enter a unique file name for the backup set.
Backup Options dialog box
Property |
Description |
Backup set name prefix |
Type the text that you want to add to the beginning of the file name to help identify the backup set. |
Backup set name suffix |
Type the text that you want to add to the end of the file name to help identify the backup set. |
![]() |
Click to include all the listed EcoStruxure BMS servers in the backup operation. You can also manually include or exclude an EcoStruxure BMS server using the Include check box. |
![]() |
Click to exclude all the EcoStruxure BMS servers selected for the backup operation. |
![]() |
Click to add the same backup set description entered for one EcoStruxure BMS server to all the other backup sets, such as Final Configuration. |
![]() |
Click to add the same content type chosen for one EcoStruxure BMS server to all the other backup sets, such as Configuration only. |
![]() |
Click to add both the backup set desciption and content type chosen for one EcoStruxure BMS server to all the other backup sets, such as Final Configuration and Configuration only. |
Server name |
Displays the name of the EcoStruxure BMS server. |
Include |
Select the EcoStruxure BMS servers that you want to include in the backup. |
Backup set name |
Displays the name of the backup set that you entered. |
Backup content |
Select the type of data that you want to back up for the EcoStruxure BMS server:
|
Backup set description |
Type a backup comment up to 255 characters that helps identify the type, content, or purpose of the scheduled backup. |