earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Functionalities: Trends
Product version: 1.9
12/14/2016

Scrolling the Trend Chart X-Axis to the Current Time

You scroll the x-axis rightmost point for fast navigation to the current time. This is useful when live update is disabled.

Show More
action_close

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic

Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic

One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic

Grid lines, schematic

To scoll the trend chart x-axis to current time
  1. In WorkStation, in the System Tree pane, select the trend chart you want to show.

  2. On the Trend Chart navigation bar, click the Scroll to current client time button

     
    action_zoom_plus_stroke
    .

The trend chart displays the trend chart with the client’s current time as the rightmost x-axis point.

  • Trend Chart Axes
  • Trend Chart Event Icons
  • Trend Chart View