Functionalities: Schedules
Product version: 3.2, 3.3, 2022
10/15/2020

Calendar Properties – Basic Tab

Use the ​ Basic tab to display general and status information about the calendar. On this tab, you can reference a lead calendar so you can reuse the events configured in the lead calendar in several shadow calendars.

 
action_zoom_plus_stroke Basic tab

Basic tab

Table: Basic Tab

Component

Description

Value

Displays True when the current date matches the date specified in the calendar entry in the Date List .

Remove past events

Select True if you want to remove calendar entries that are older than 60 days.

Lead object

Select a lead calendar if you are creating a shadow calendar.

  • General Information Properties – Basic Tab
  • References Tab