You can configure the unit for a value and force or change values.
Using the Configure dialog box and the Configuration tab you can change or set units for values.
Component |
Description |
Type |
Displays the object type. Read-only |
Unit |
Displays the Unit. Select to change the unit. For more information, see Units . |
Init value |
Displays the Init value. |
Reference |
Displays the Reference. |
Forceable |
Select to make the value forcible. For more information, see Forced Values . |
Retain level |
Select how to handle values for warm start, cold start, system events, and system activities. For more information, see Retain Level . |
Null |
Select the Null checkbox, to remove any value of a property. The Null checkbox is available for all properties where the value can be removed. For example, you can remove references from trend logs using the Null checkbox. |
Values can be forced to a certain value. The true value from the system is displayed in the Unforced value box.