earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
12/14/2016

Configuring the Acknowledgement Type of an Alarm

You configure the properties of an alarm to meet the unique needs of your site.

To configure the acknowledgement type of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. Click the User Action tab.

  3. Select the Aknowledgement type :

    • Click No when the alarm does not need to be acknowledged.

    • Click Single when the alarm needs to be acknowledged in the alarm state.

    • Click Extended when the alarm needs to be acknowledged in the alarm state and the reset state.

     
    action_zoom_plus_stroke
  4. In the Changes have been made dialog box, click Yes to save the changes.

  • Create Alarm Wizard – User Action Page
  • Acknowledgements